Write/Read |
About Exporting Data |
Description |
Sets and reads the number of ports for which data will be exported. This selection appears on the DUT Configuration "Change" dialog.
To export data, use ExportFreqDomainTextFileWithSpecifiedDefaults Method or ExportTimeDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportPortNmbr = value |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
value |
(Integer) Number of ports to export. Select the same or less than the number of ports in the original data. If less than the original data, some parameters will NOT be exported. |
Return Type |
Integer |
Default |
-1 - Export data for ALL of the original ports. |
Examples |
doc.ExportPortNmbr = 2 |
C++ Syntax |
HRESULT get_ExportPortNmbr(long *Value); HRESULT put_ExportPortNmbr(long Value); |
Interface |
IPLTSDoc |