Write/Read |
About Exporting Data |
Description |
Sets and reads the type of text file to export. To export data, use ExportFreqDomainTextFileWithSpecifiedDefaults Method or ExportTimeDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportTextFileDelimiter = value |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
value |
(Enum as pltsTextFileDelimiter) Delimiter. Choose from: 0 - Tab 1 - Comma |
Return Type |
Enum |
Default |
Tab |
Examples |
doc.ExportTextFileDelimiter = Comma |
C++ Syntax |
HRESULT get_ExportTextFileDelimiter(tag pltsTextFileDelimiter *Value); HRESULT put_ExportTextFileDelimiter(tag pltsTextFileDelimiter); |
Interface |
IPLTSDoc |