Write/Read |
About Exporting Data |
Description |
Sets and reads the units to use when exporting Time domain data. To export data, use ExportTimeDomainTextFileWithSpecifiedDefaults Method. |
VB Syntax |
doc.ExportTimeUnit = value |
Variable |
(Type) - Description |
|
doc |
(object) - A PLTSDoc object |
|
value |
(Enum as pltsTimeUnits) Units in which data will be exported. Choose from: 0 - ns (nanoseconds) 1 - cm (centimeters) |
Return Type |
Enum |
Default |
0 - ns |
Examples |
doc.ExportTimeUnit = cm |
C++ Syntax |
HRESULT get_ExportTimeUnit(tag pltsTimeUnits *Value); HRESULT put_ExportTimeUnit(tag pltsTimeUnits Value); |
Interface |
IPLTSDoc |