Write-only |
About User Preferences |
Description |
Load the specified user preferences file. |
VB Syntax |
plts.LoadUserPreferences fileName |
Variable |
(Type) - Description |
|
plts |
(object) - A PLTSApplication object |
|
fileName |
(String) Full path, filename, and suffix of the user preference file to be loaded. |
Return Type |
None |
Default |
None |
Examples |
pltsapp.LoadUserPreferences "C://Program Files//Keysight//PLTS_4.0//System//Default.prf" |
C++ Syntax |
HRESULT LoadUserPreferences(BSTR prfName); |
Interface |
IPLTSApplication |