Write-only |
About User Preferences |
Description |
Create a new measurement using the default user preference settings. |
VB Syntax |
plts.NewFile fileName, analysistype, IDoc, IView |
Variable |
(Type) - Description |
|
plts |
(object) - A PLTSApplication object |
|
fileName |
(String) File name of the new measurement. |
|
analysisType |
(Short) Analysis view that is displayed after the new file is created. Provide either the number or enumeration type depending on your programming environment. 0 - TIME_DIFF (Time domain differential) 1 - TIME_SNGL (Time domain single-ended) 2 - FREQ_BAL (Frequency domain balanced) 3 - FREQ_SNGL (Frequency domain single-ended) 4 - EYE_DIFF (Eye diagram differential) 5 - EYE_SNGL (Eye diagram single-ended) 6 - RLCGD (RLCG differential) 7 - RLCGC (RLCG common) 8 - RLCGWE (RLCG W element) 9 - RLCGSM (RLCG self mutual) |
|
IDoc |
[out] Returns a handle to the new IPLTSDocument object. |
|
IView |
[out] Returns a handle to the new IPLTSView object. |
Return Type |
Object |
Default |
None |
Examples |
plts.NewFile "MyDUT", TIME_DIFF, iDoc, iView |
C++ Syntax |
HRESULT NewFile(BSTR fileName, SHORT analysisType, IDispatch** ppDoc, IDispatch** ppView); |
Interface |
IPLTSApplication |