N1957A Test System or N4421A Test Set with E8364A Network Analyzer
N4420B Test Set with E8363A Network Analyzer Interconnections
N1953A Test System or N4419A Test Set with E8362A Network Analyzer
N1951A Test System or N4418A Test Set with 8720ES or 8722ES Network Analyzer
N4416A Test Set with the E8356A, E8357A, or E8358A Network Analyzer
|
The Reference channel path through the test set is used to compensate for electrically-long DUTs. This also results in added loss in the Reference channel and higher trace noise. Therefore, unless making high-speed measurements of electrically-long devices, do NOT remove the PNA REFERENCE 1 and REFERENCE 2 front-panel loops, and do NOT use the Reference channel interconnect cables (items 1, 2, 3, 4, 13, and 14). |
Specifications for Discontinued Systems
Front and Rear Panels for Discontinued Systems
Note: When connecting the interconnect cables described in this topic, be careful to install the interconnect cables correctly. The longer end of the interconnect cable connects to the network analyzer front panel connector.
|
|
If the test set and the network analyzer are rack mounted, the screws securing the rack mount flanges to the instrument rack may be loosened slightly to allow for minor repositioning of the instruments. Don't forget to retighten the screws when you are done.
|
|
2. CAUTION Damage to the interconnect cable can result from improper orientation of the cable. Learn about correct cable orientation.
|
Call Out |
Cable Part Number |
From |
To |
|
1 |
Z5623-20215 |
REF 1 SOURCE OUT |
REF 1 R1 OUT |
|
2 |
Z5623-20215 |
REF 1 RCVR R1 IN |
REF 1 RCVR R1 IN |
|
3 |
Z5623-20215 |
REF 2 RCVR R2 IN |
REF 2 RCVR R2 IN |
|
4 |
Z5623-20215 |
REF 2 SOURCE OUT |
REF 2 R2 OUT |
|
5 |
Z5623-20216 |
PORT 1 SOURCE OUT |
PORT 1 SOURCE OUT |
|
6 |
Z5623-20216 |
PORT 1 CPLR THRU |
PORT 1 CPLR THRU |
|
7 |
Z5623-20216 |
PORT 2 CPLR THRU |
PORT 2 CPLR THRU |
|
8 |
Z5623-20216 |
PORT 2 SOURCE OUT |
PORT 2 SOURCE OUT |
|
9 |
Z5623-20217 |
PORT 1 CPLR ARM |
PORT 1 CPLR ARM |
|
10 |
Z5623-20217 |
PORT 1 RCVR A IN |
PORT 1 RCVR A IN |
|
11 |
Z5623-20217 |
PORT 2 RCVR B IN |
PORT 2 RCVR B IN |
|
12 |
Z5623-20217 |
PORT 2 CPLR ARM |
PORT 2 CPLR ARM |
|
13 |
E8364-20059 |
REF 1 on rear panel of the test set |
|
|
14 |
E8364-20059 |
REF 2 on rear panel of the test set |
|
|
|
2. CAUTION Damage to the interconnect cable can result from improper orientation of the cable. Learn about correct cable orientation.
|
Call Out |
Cable Part Number |
From |
To |
|
1 |
Z5623-20215 |
REF 1 SOURCE OUT |
REF 1 R1 OUT |
|
2 |
Z5623-20215 |
REF 1 RCVR R1 IN |
REF 1 RCVR R1 IN |
|
3 |
Z5623-20215 |
REF 2 RCVR R2 IN |
REF 2 RCVR R2 IN |
|
4 |
Z5623-20215 |
REF 2 SOURCE OUT |
REF 2 R2 OUT |
|
5 |
Z5623-20216 |
PORT 1 SOURCE OUT |
PORT 1 SOURCE OUT |
|
6 |
Z5623-20216 |
PORT 1 CPLR THRU |
PORT 1 CPLR THRU |
|
7 |
Z5623-20216 |
PORT 2 CPLR THRU |
PORT 2 CPLR THRU |
|
8 |
Z5623-20216 |
PORT 2 SOURCE OUT |
PORT 2 SOURCE OUT |
|
9 |
Z5623-20217 |
PORT 1 CPLR ARM |
PORT 1 CPLR ARM |
|
10 |
Z5623-20217 |
PORT 1 RCVR A IN |
PORT 1 RCVR A IN |
|
11 |
Z5623-20217 |
PORT 2 RCVR B IN |
PORT 2 RCVR B IN |
|
12 |
Z5623-20217 |
PORT 2 CPLR ARM |
PORT 2 CPLR ARM |
|
13 |
E8364-20059 |
REF 1 on rear panel of the test set |
|
|
14 |
E8364-20059 |
REF 2 on rear panel of the test set |
|
|
|
2. CAUTION Damage to the interconnect cable can result from improper orientation of the cable. Learn about correct cable orientation.
|
Call Out |
Cable Part Number |
From |
To |
|
1 |
AD00756-1 |
REF 1 SOURCE OUT |
REF 1 SOURCE OUT |
|
2 |
AD00756-1 |
REF 1 RCVR R1 IN |
REF 1 RCVR R1 IN |
|
3 |
AD00756-1 |
REF 2 RCVR R2 IN |
REF 2 RCVR R2 IN |
|
4 |
AD00756-1 |
REF 2 SOURCE OUT |
REF 2 SOURCE OUT |
|
5 |
AD00756-2 |
PORT 1 SOURCE OUT |
PORT 1 SOURCE OUT |
|
6 |
AD00756-2 |
PORT 1 CPLR THRU |
PORT 1 CPLR THRU |
|
7 |
AD00756-2 |
PORT 2 CPLR THRU |
PORT 2 CPLR THRU |
|
8 |
AD00756-2 |
PORT 2 SOURCE OUT |
PORT 2 SOURCE OUT |
|
9 |
AD00756-3 |
PORT 1 CPLR ARM |
PORT 1 CPLR ARM |
|
10 |
AD00756-3 |
PORT 1 RCVR A IN |
PORT 1 RCVR A IN |
|
11 |
AD00756-3 |
PORT 2 RCVR B IN |
PORT 2 RCVR B IN |
|
12 |
AD00756-3 |
PORT 2 CPLR ARM |
PORT 2 CPLR ARM |
|
13 |
AD00756-4 |
REF 1 on rear panel of the test set |
|
|
14 |
AD00756-4 |
REF 2 on rear panel of the test set |
|
|
|
2. CAUTION Damage to the interconnect cable can result from improper orientation of the cable. Learn about correct cable orientation.
|
Call Out |
Cable Part Number |
From |
To |
|
1 |
AD00599-2 |
PORT 1 SWITCH |
PORT 1 SWITCH |
|
2 |
AD00599-1 |
A IN |
A IN |
|
3 |
AD00599-2 |
PORT 1 BIAS TEE |
PORT 1 COUPLER |
|
4 |
AD00599-1 |
A OUT |
A OUT |
|
5 |
AD00599-2 |
PORT 2 BIAS TEE |
PORT 2 COUPLER |
|
6 |
AD00599-1 |
B OUT |
B OUT |
|
7 |
AD00599-4 |
R CHANNEL OUT |
R OUT |
|
8 |
AD00599-3 |
R CHANNEL IN |
R IN |
|
9 |
AD00599-2 |
PORT 2 SWITCH |
PORT 2 SWITCH |
|
10 |
AD00599-1 |
B IN |
B IN |
|
11 |
AD00599-5 |
REF 1 on rear panel of the test set |
|
(or N4417A Option 104 Test Set with E8356A, E8357A, or E8358A Network Analyzer)
|
|
2. CAUTION Damage to the interconnect cable can result from improper orientation of the cable. Learn about correct cable orientation.
|
Installation |
Cable |
From |
To |
|
1 |
AD00653-2 |
R1 IN |
R1 IN |
|
2 |
AD00653-2 |
A IN |
A IN |
|
3 |
AD00653-2 |
COUPLER IN |
COUPLER IN |
|
4 |
AD00653-2 |
COUPLER IN |
COUPLER IN |
|
5 |
AD00653-2 |
B IN |
B IN |
|
6 |
AD00653-2 |
R2 IN |
R2 IN |
|
7 |
AD00653-1 |
R1 OUT |
R1 OUT |
|
8 |
AD00653-1 |
A OUT |
A OUT |
|
9 |
AD00653-1 |
SOURCE OUT |
SOURCE OUT |
|
10 |
AD00653-1 |
SOURCE OUT |
SOURCE OUT |
|
11 |
AD00653-1 |
B OUT |
B OUT |
|
12 |
AD00653-1 |
R2 OUT |
R2 OUT |
|
13 |
AD00653-3 |
REF 1 on rear panel of the test set |
|
|
14 |
AD00653-3 |
REF 2 on rear panel of the test set |
|
(or N4417A Option 103 Test Set with E8801A, E8802A, or E8803A Network Analyzer)
|
|
2. CAUTION Damage to the interconnect cable can result from improper orientation of the cable. Learn about correct cable orientation.
|
Installation |
Cable |
From |
To |
|
1 |
AD00653-2 |
R1 IN |
R1 IN |
|
2 |
AD00653-2 |
A IN |
A IN |
|
3 |
AD00653-2 |
COUPLER IN |
COUPLER IN |
|
4 |
AD00653-2 |
COUPLER IN |
COUPLER IN |
|
5 |
AD00653-2 |
B IN |
B IN |
|
6 |
AD00653-1 |
R1 OUT |
R1 OUT |
|
7 |
AD00653-1 |
A OUT |
A OUT |
|
8 |
AD00653-1 |
SOURCE OUT |
SOURCE OUT |
|
9 |
AD00653-1 |
SOURCE OUT |
SOURCE OUT |
|
10 |
AD00653-1 |
B OUT |
B OUT |
|
11 |
AD00653-3 |
REF 1 on rear panel of the test set |
|
|
|
2. CAUTION Damage to the interconnect cable can result from improper orientation of the cable. Learn about correct cable orientation.
|
Installation |
Cable |
From |
To |
|
1 |
AD00653-2 |
R1 IN |
R1 IN |
|
2 |
AD00653-2 |
A IN |
A IN |
|
3 |
AD00653-2 |
COUPLER IN |
COUPLER IN |
|
4 |
AD00653-2 |
COUPLER IN |
COUPLER IN |
|
5 |
AD00653-2 |
B IN |
B IN |
|
6 |
AD00653-2 |
R2 IN |
R2 IN |
|
7 |
AD00653-1 |
R1 OUT |
R1 OUT |
|
8 |
AD00653-1 |
A OUT |
A OUT |
|
9 |
AD00653-1 |
SOURCE OUT |
SOURCE OUT |
|
10 |
AD00653-1 |
SOURCE OUT |
SOURCE OUT |
|
11 |
AD00653-1 |
B OUT |
B OUT |
|
12 |
AD00653-1 |
R2 OUT |
R2 OUT |
|
13 |
AD00653-3 |
REF 1 on rear panel of the test set |
|
|
14 |
AD00653-3 |
REF 2 on rear panel of the test set |
|