The following hardware is discontinued. However, in addition to this topic,the following documentation is still provided:
|
Discontinued PLTS Hardware Model Numbers |
|
|
PLTS Systems: |
N1947A, N1948A, N1951A, N1953A, N1957A |
|
PLTS Test Sets: |
N4415A, N4416A, N4417A, N4418A, N4419A, N4421A |
|
PLTS Network Analyzers: |
8753ES 8720ES/8722ES E8356A/E8357A/E8358A E8362A/E8363A/E8364A E8801A/E8802A/E8803A |
|
Test Set |
System |
Network Analyzer |
|||
|---|---|---|---|---|---|
|
Model |
Options1 |
||||
|
Required |
Compatible |
Incompatible |
|||
|
N4415A |
30 kHz to 6.0 GHz |
8753ES |
0062, 014 |
002, 004, 010, 1D5 |
011, 075, H16 |
|
N4416A |
300 kHz to 6.0 GHz |
E8356A3/7A/8A |
015 |
010, 1D5 |
|
|
N4417A4 |
300 kHz to 9.0 GHz |
E8356A3/7A5/8A |
015 |
010 |
|
|
E8801A4/2A/3A |
014 |
010, 1E1, 1E5 |
|
||
|
N4418A |
50 MHz to 20 GHz |
8720ES |
H32 or H42 |
010, 012, 400 |
007, 085, 089 |
|
8722ES6 |
H32 or H44 |
||||
|
N4419A |
45 MHz to 20 GHz |
E8362A |
014 |
010, 022, 711, UNL |
|
|
N4420B |
45 MHz to 40 GHz |
E8363A |
014 |
010, 022, 711, UNL |
|
|
N4421A |
45 MHz to 50 GHz |
E8364A |
014 |
010, 022, 711, UNL |
|
|
1 This table lists only the most specifically relevant options. For compatibility with options not listed here, contact the factory. 2 Option 006 required only for operation above 3 GHz. 3 Using this network analyzer, the maximum operating frequency is limited to 3 GHz. 4 E8356A family requires N4417A Option 103; E8801A family requires N4417A Option 104. 5 Using this network analyzer, the maximum operating frequency is limited to 6 GHz. 6 When an 8722ES is used with an N4418A, the N4418A requires Option 302. The system's maximum operating frequency is limited to 20.0 GHz. |
Note: For PNA models E8356A/E8357A/E8358A: If the rear panel USB port is oriented horizontally, then you have an older CPU board. We strongly recommend that you install 128 MB of memory if any firmware revision above 2.62 is desired. While this is not an absolute necessity, performance will be very sluggish without this extra memory. Even with this extra memory, using more than 1601 points will slow the responsiveness of the analyzer. The memory type needed is: 128MB SDRAM SODIMM, PC66 or PC100.
Using the following table, verify that your network analyzer options are compatible with the physical layer test system. Incompatible options are shaded.
|
8753ES Network Analyzer Options |
|||
|
002 |
Harmonic-Measurement Upgrade |
004 |
Step Attenuator Upgrade |
|
006 |
6 GHz Upgrade for Standard Units |
010 |
Time Domain Capability |
|
011 |
Receiver Configuration |
014 |
Configurable Test Set |
|
075 |
75 Ohm Impedance |
1D5 |
High Stability Frequency Reference |
|
H16 |
Low Noise Floor |
|
|
|
8720ES and 8722ES Network Analyzer Options |
|||
|
007 |
Mechanical Transfer Switch |
010 |
Time Domain Capability |
|
012 |
Direct Sampler Access |
085 |
High-Power Test System |
|
089 |
Frequency Offset Mode |
1D5 |
High Stability Frequency Reference |
|
400 |
Four-Sampler Test Set |
H32 |
Front panel access to A and B samplers and Port 1 and Port 2 switch and coupler |
|
H42 |
8719/8720 only: Front panel access to all samplers and Port 1 and Port 2 switch and coupler (installs options 400 & 012) |
H44 |
8722 only: Front panel access to R1, R2, A, and B samplers, and Port 1 and Port 2 switch and coupler ports (installs options 400 & 012) |
|
E8356A, E8357A, and E8358A Network Analyzer Options1 |
|||
|
010 |
Time Domain Capability |
015 |
Configurable Test Set |
|
E8801A, E8802A, and E8803A Network Analyzer Options1 |
|||
|
010 |
Time Domain Capability |
014 |
Configurable Test Set |
|
1E1 |
Extended Power Range |
1E5 |
High Stability Timebase |
|
E8362A, E8363A, and E8364A Network Analyzer Options1 |
|||
|
010 |
Time Domain Capability |
014 |
Configurable Test Set |
|
0162 |
Add Receiver Attenuators |
022 |
Extended Memory |
|
0802 |
Frequency Offset |
0812 |
External Reference Switch |
|
0832 |
Frequency Converter Measurement Application |
711 |
Standard Power Range |
|
UNL |
Extended Power Range with Bias Tees |
|
|
|
1 Network analyzer should have firmware revision A.03.53 or later. Contact the factory for information regarding PLTS support of earlier firmware revisions. 2 This option has not been tested and is not specified with the Physical Layer Test System. |