Data Sharing allows you to view traces from different files with different measurement setup parameters on a single plot. This is very helpful when comparing a parameter from the current measurement with the same parameter from a previous measurement that you made.
Beginning with PLTS revision 4.0, data sharing has become much simpler. See how to open multiple traces from different data files on the same plot.