This example iterates over the entire collection of Cal Sets that currently reside in the PNA. It reads the entire list of error term strings from each Cal Set and queries the data for each term. It then does the same for the standards data.
Learn more about Reading and Writing Calibration data using COM.
Learn more about Cal Sets.
See example: Writing Cal Set Data using COM
See Other COM Example Programs
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save on the PNA hard drive as CalSets.vbs. Learn how to setup and run the macro.
Dim pna
Dim cset
Dim calsets
' create the pna object
' to run on a remote PC, substitute 'name' for the full computer name of your PNA
' to run as a macro on the PNA, remove ,"name"
Set pna = CreateObject("AgilentPNA835x.Application", "name")
wscript.echo pna.IDString
' obtain the calset collection
Set calsets = pna.GetCalManager.calsets
' loop thru the calsets
Dim c
For c = 1 To calsets.count
Set cset = calsets.Item(c)
' wscript.echo prints values to a message box
wscript.echo "calset = ", cset.GetGUID, cset.Description
' iterate through error terms data
Dim vterms,fdata
vterms = cset.GetErrorTermList2(0, "")
if (Not IsEmpty(vterms)) then
For i = LBound(vterms) To UBound(vterms)
wscript.echo vterms(i)
vdata = cset.GetErrorTermByString(0,vterms(i))
fdata = cset.GetErrorTermStimulus(0,vterms(i))
wscript.echo vdata(1,0), vdata(1,1)
wscript.echo fdata(1,0), fdata(1,1)
Next
end if
' iterate through standards data
vterms = cset.GetStandardList2("")
if (Not IsEmpty(vterms)) then
For i = LBound(vterms) To UBound(vterms)
wscript.echo vterms(i)
vdata = cset.GetStandardByString( vterms(i) )
wscript.echo vdata(1,0), vdata(1,1)
Next
end if
Next
Last modified:
|
2-May-2011 |
Added GetErrorTermStimulus |