This VBScript example creates a calibrated SMC fixed output measurement using a controlled LO. Then a single sweep is taken and data is retrieved.
Requirements:
If an external LO is used, it should be configured to match the LOName property of the mixer object.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as SMC.vbs. Learn how to setup and run the macro.
| 
 option explicit ' Utility function function ToString(complexDataArray) dim dataAsString dim point for point = 0 to UBound(data) dataAsString = dataAsString & "(" & data(point,0) & "," & data(point,1) & ") " next ToString = dataAsString end function dim app set app = createobject("agilentpna835x.application") app.preset ' Put the channel in hold (highly recommended) app.ActiveChannel.Hold 1 ' Delete the standard measurement app.ActiveMeasurement.Delete ' Create an SC21 measurement app.CreateCustomMeasurementEx 1, "Scalar Mixer/Converter","SC21" ' Set the number of points to 11 app.ActiveChannel.NumberOfPoints = 11 ' Setup the mixer parameters for a swept LO, fixed output measurement dim mixer set mixer = app.ActiveMeasurement mixer.InputStartFrequency = 200e6 mixer.InputStopFrequency = 700e6 mixer.LORangeMode(1) = 0 ' 0 = Swept mode mixer.OutputFixedFrequency = 3.4e9 mixer.InputPower = -17 mixer.LOPower(1) = 10 'mixer.LOName(1) = "8360" ' The CALCULATE method calculates the LO frequency from the other parameters, ' It also applies ALL mixer parameters to the channel. mixer.Calculate 3 ' Calculate the LO range ' Create an S11 in the same channel app.CreateCustomMeasurementEx 1, "Scalar Mixer/Converter","S11" dim S11Meas set S11Meas = app.ActiveMeasurement ' Create an IPwr in the same channel app.CreateCustomMeasurementEx 1, "Scalar Mixer/Converter","IPwr" ' Create an OPwr in the same channel app.CreateCustomMeasurementEx 1, "Scalar Mixer/Converter","OPwr" ' Perform a single sweep synchronously. app.ActiveChannel.Single 1 ' Retrieve the SC21 data dim data 'Get the calibrated values in polar format data = mixer.GetData(1,3) ' 1 = naCorrectedData, 3 = naDataFormat_Polar wscript.echo "SC21=" & ToString(data) ' Retrieve the S11 data 'Get the calibrated values in polar format data = S11Meas.GetData(1,3) ' 3 = naDataFormat_Polar wscript.echo "S11=" & ToString(data)  | 
Last Modified:
| 
 8-Mar-2011  | 
 Updated for A.09.33  | 
| 
 13-June-2006  | 
 Last updated  |