This example creates and calibrates an SMC measurement. A power sensor must first be connected to the PNA.
By removing the comments ( ' ) at the start of the BLUE code, it can also do the following:
Load a Mixer setup file from the PNA at: C:/Program Files/Keysight/Network Analyzer/Documents/Mixer/MyMixer.mxr.
Cal using an ECal module.
Perform manual ECAL orientation
Load a Phase Reference calibration.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save on the PNA hard drive as SMC.vbs. Learn how to setup and run the macro.
Create an SMC Fixed Output Meas
Use Existing Power Cal for SMC
|
Dim App Set App = CreateObject("AgilentPNA835x.Application") App.Preset Dim Meas Set Meas = App.ActiveMeasurement Meas.Delete App.CreateCustomMeasurementEx 1, "Scalar Mixer/Converter","SC21" 'Other valid strings that can be specified to create a measurement with a parameter 'other than'"SC21" are: "S11", "S22", "IPwr", and "OPwr" dim chan set chan = app.activechannel 'Attenuator setting must match optional Phase Ref Cal setting chan.attenuator(1) = 10 chan.NumberOfPoints = 11 chan.IFBandwidth = 1000 'You can perform mixer setup here or 'recall a previous mixer setup from the PNA Hard drive. 'This is how to perform mixer setup using IConverter. ' Setup Stimulus dim cv set cv = chan.Converter cv.InputStartFrequency = 3.6e9 cv.InputStopFrequency = 4.9e9 cv.LOFixedFrequency(1) = 1e9 cv.LOPower(1) = 10 cv.OutputSideband = 0 'Lowside cv.Calculate 2 'Calc output 'cv.EnablePhase = True cv.LOName(1)="Port 3" cv.Apply()
' Alternatively, recall a mixer setup from the PNA Hard drive 'Meas.LoadFile "C:/Program Files/Keysight/Network Analyzer/Documents/Mixer/MyMixer.mxr"
' Begin Calibration Dim CalMgr Set CalMgr = App.GetCalManager Dim SMC Set SMC = CalMgr.CreateCustomCal("SMC") SMC.Initialize 1, 1 SMC.ConnectorType(1) = "APC 3.5 male" SMC.ConnectorType(2) = "APC 3.5 female" ' Use Mechanical cal kits SMC.CalKitType(1) = "85033D/E" SMC.CalKitType(2) = "85033D/E" ' To use an ECal module instead, comment out the above two lines ' and uncomment the appropriate lines below: ' Your ECal module must already be connected ' via USB to the PNA. ' SMC.CalKitType(1) = "N4691-60004 ECal" ' SMC.CalKitType(2) = "N4691-60004 ECal" ' Non-factory characterizations are specified as follows: ' SMC.CalKitType(1) = "N4691-60004 User 1 ECal" ' When two or more ECal modules with the same model number are connected ' also specify the serial number as follows: ' SMC.CalKitType(1) = "N4691-60004 ECal 01234" ' When Disk Memory ECal user characterizations are used, ' specify both the User char and the serial number as follows: ' SMC.CalKitType(1) = "N4691-60004 MyDskChar ECal 01234" ' Turn on auto orientation for the ECal (default behavior). ' SMC.AutoOrient = 1' MsgBox("Cal kits defined for Ports 1 and 2") ' Import power cal data from an existing SMC calset. ' This calset MUST exist on the PNA. SMC.ImportDataSet "Phase Reference-full-span","POWER_AND_PHASE" 'Omit the isolation part of the 2-port cal (default behavior). SMC.OmitIsolation = 1
Dim steps steps = SMC.GenerateSteps For i = 1 To steps MsgBox SMC.GetStepDescription(i) SMC.AcquireStep i Next Dim calset calset = SMC.GenerateErrorTerms Msgbox("SMC Cal Complete!") |
Last Modified:
|
8-Mar-2012 |
Edit for LOName (ZW) |
|
24-Feb-2012 |
Added Phase Ref option |
|
5-Apr-2011 |
Edited for ECal options |
|
8-Mar-2011 |
Updated for A.09.33 |