This VBScript example modifies display colors, modifies trace1 colors, then saves and recalls the theme.
These programs can be run as a macro in the PNA. To do this, copy the code into a text editor file such as Notepad and save on the PNA hard drive as Colors.vbs. Learn how to setup and run the macro.
|
function RGB(R, G, B) RGB = R + G*(2^8) + B*(2^16) end Function
shell.AppActivate "PNA Series Network Analyzer" Set app = CreateObject("AgilentPNA835X.Application") app.preset Set colors = app.Preferences.DisplayColors ' Uncomment the following line to modify Print colors ' Set colors = app.Preferences.PrintColors colors.ResetTheme( ) colors.background = RGB(64,0,64) ' purple displaycolors.grid = RGB(0,255,128) ' greenish colors.activeLabels = RGB(0,0,255) ' blue colors.inactiveLabels = RGB(255,0,0) ' red colors.failedTraces = RGB(255,128,64) ' orange dim Trace1 Set Trace1 = colors.Trace(1) Trace1.DataAndLimits = RGB(1,251,1) ' green Trace1.Memory = RGB(251,1,1) ' red Trace1.Markers = RGB(251,251,251) ' white Trace1.MemoryMarkers = RGB(1,251,251) ' green + blue colors.StoreTheme("c:/Program Files/Keysight/Network Analyzer/Colors/Theme1.colors") colors.LoadTheme("c:/Program Files/Keysight/Network Analyzer/Colors/Theme1.colors") |