This example sets up an SMC channel and a standard channel. It then performs a 'Cal All Channels' calibration which calibrates both channels.
Note: The example does NOT modify any path configuration settings.
|
'Access the CalAllChannels object Dim app Set app = CreateObject("AgilentPNA835x.Application") Dim mgr Set mgr = app.GetCalManager 'Preset PNA app.Preset '********** Setup Channel 1, Window 1 ********** ' Get a handle to the preset channel 1 set meas1=app.ActiveMeasurement set chan1=app.ActiveChannel set win1=app.ActiveNAWindow 'Modify stimulus settings 'Set IF Bandwidth to 1kHz chan1.IFBandwidth = 1e3 'Set Center and Span Freq's to 1 GHz chan1.CenterFrequency = 1e9 chan1.FrequencySpan = 1e9 'Set number of points to 11 chan1.NumberOfPoints = 11 ' '********** Setup SMC in Channel 2 in new window********** app.CreateCustomMeasurementEx 2, "Scalar Mixer/Converter","SC21",2 Set smcChan = app.ActiveChannel smcChan.NumberOfPoints = 11 smcChan.IFBandwidth = 1e3 ' the rest are Mixer settings dim mixer set mixer = app.ActiveMeasurement mixer.InputRangeMode = 0 'swept Input mixer.InputStartFrequency = 3.6e9 mixer.InputStopFrequency = 3.9e9 mixer.LORangeMode(1) = 1 'fixed LO mixer.LoFixedFrequency(1) = 1e9 mixer.LOPower(1) = 10 mixer.LOName(1) = "Port 3" mixer.OutputSideband = 1 'Low side mixer.Calculate 2 'Calc Output mixer.Apply ' '********** Setup CalAll Channel Dim CalAll Set CalAll = mgr.CalibrateAllChannels 'Reset Cal All settings CalAll.Reset 'Select the channels to cal 'VMC channels are not supported by Cal All. CalAll.Channels = Array(1,2) 'Set IFBW CalAll.IFBW = 1e3 'Set power level for port 1 CalAll.PowerLevel(1) = 0 'Set CalSet prefix. The channel number is appended to 'the User Cal set for each channel. 'If you don’t set this, only Cal Registers will be generated. calAll.UserCalsetPrefix = "MyCalAll" ' Read unique Cal settings for Cal All channels props = calAll.PropertyNames msg = "calAll.PropertyNames:" & vbCrLf For i = 0 to UBound(props) msg = msg & " " & CStr(i) & ". " & props(i) & vbCrLf Next resp = MsgBox(msg) ' We want "Enable Phase Correction" ' Now find valid settings propName = "Enable Phase Correction" uniqVal = calAll.PropertyValues (propName) 'returns 'false,true' make it true. For i = 1 to UBound(uniqVal) MsgBox "calAll.PropertyValues (" & propName & ") = " & uniqVal(i) Next calAll.PropertyValue(propName) = "true" ' '********* 'Perform Guided Cal ******* ' Get a handle to the GuidedCal object Dim guidedcal set guidedcal = calAll.GuidedCalibration ' Specify the DUT connectors guidedcal.ConnectorType(1) = "APC 3.5 male" guidedcal.ConnectorType(2) = "APC 3.5 male" guidedcal.ConnectorType(3) = "Not used" guidedcal.ConnectorType(4) = "Not used" MsgBox "Connectors defined for Ports 1 and 2" ' Select the Cal Kit for each port being calibrated. guidedCal.CalKitType(1) = "85052D" guidedCal.CalKitType(2) = "85052D" MsgBox "Cal kits defined for Ports 1 and 2" ' Initiate the calibration and query the number of steps Numsteps = guidedcal.GenerateSteps For i = 1 to Numsteps step = "Step " + CStr(i) + " of " + CStr(Numsteps) strPrompt = guidedCal.GetStepDescription(i) value = MsgBox(strPrompt, vbOKOnly, step) guidedCal.AcquireStep i Next ' Conclude the calibration guidedCal.GenerateErrorTerms csets = calAll.GeneratedCalSets For i = 0 to UBound(uniqVal) MsgBox (csets(i)) Next |
Last modified:
|
9-Jan-2012 |
New topic |