This example performs a user-characterization and stores it to both the ECal module memory and PNA disk memory.
It then performs two 2-port cals: the first using the characterization from module memory, then using the characterization from disk memory.
Note: This example requires that channel 1 be already calibrated.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file, such as Notepad, and save it on the PNA hard drive as ECal.vbs.
How to setup and run the macro.
See Other COM Example Programs
|
Option Explicit Dim pna Set pna = CreateObject("AgilentPNA835x.Application") Dim calMgr Set calMgr = pna.GetCalManager ' Get ECal User Characterizer COM object Dim ecalCharacterizer Set ecalCharacterizer = calMgr.GetECalUserCharacterizer ' Substitute here the model number and serial number of your own ECal. ' Note that this example corresponds to a 4-port ECal module with ' serial number 00001. If instead you have a 2-port ECal module, ' their model numbers are '5x5' numbers -- for example, 'N4691-60001'. Dim ecalModelNum ecalModelNum = "N4433A" Dim ecalSerialNum ecalSerialNum = "00001" ecalCharacterizer.ECalID = ecalModelNum & "," & ecalSerialNum MsgBox "ECal module to be characterized is: " & ecalCharacterizer.ECalID ' Set which user characterization number (1-12) the new characterization ' will be stored to in the ECal module when it is done. If you intend to ' store your user characterization just to PNA Disk Memory and NOT the ' ECal module's memory, then omit the setting of this property. ecalCharacterizer.CharacterizationNumber = 1 ' The following commented-out lines of code show how you can access ' the list of connector type names you can set for the ports of an ' ECal when you user-characterize it. However, please note that if ' you are writing the user characterization to the ECal module's memory, ' as of yet only the Factory Defined set of connector choices will work ' properly (see the ValidConnectorType property). ' If you will be saving your characterization to just ' PNA Disk Memory only, then all connector names returned by this call ' will work, user-defined connector names as well as factory-defined. 'Dim connTypeArray 'connTypeArray = ecalCharacterizer.ValidConnectorTypes 'MsgBox connTypeArray(1) ' Access element 1 in the string array ' For each port of the ECal module, specify which connector type ' is at the end of the adapter (or cable or fixture) that is ' connected to that port of the ECal for the characterization ' (must be one of the connector types that is included in the ' list that the ValidConnectorTypes method returns). The default ' is "No adapter", which assumes you are characterizing that port ' of the ECal "as is" (nothing attached to it). So in this example, ' Ports C and D of the ECal are being characterized to just the ' ECal's connectors. ecalCharacterizer.ConnectorType(1) = "APC 3.5 male" ' ECal Port A ecalCharacterizer.ConnectorType(2) = "APC 3.5 male" ' ECal Port B ' As with the connector types, the information set in these next ' few properties also gets stored within the characterization. ' Set the name of the person and/or company that is producing ' this characterization. ecalCharacterizer.UserName = "John Doe, Acme Inc." ' Set user-specified description of the PNA being used. ecalCharacterizer.UserDescriptionOfPNA = "SN US12345678" ' Set descriptions of what you have connected to the ECal module's ' ports for the characterization. ecalCharacterizer.PortDescription(1) = "3.5 mm adapter, SN 00001" ' Port A of the ECal ecalCharacterizer.PortDescription(2) = "3.5 mm adapter, SN 00002" ' Port B of the ECal ' Begin a user characterization on Channel 1. ' If you will be storing this characterization to the ECal module's memory, then ' the boolean argument to this command should be set to True. If you will be storing ' this characterization to PNA disk memory ONLY, then you should specify False for ' that argument. In this example we will be storing the characterization to both ' module memory and PNA disk memory, so we use True. ecalCharacterizer.InitializeEx 1, True ' Generate the measurement steps for the user characterization. Dim numSteps numSteps = ecalCharacterizer.GenerateSteps ' Measure the steps. ' You must ensure you have already applied the appropriate calibration to the channel ' already, or else an error will be thrown indicating that. Dim i For i = 1 To numSteps MsgBox ecalCharacterizer.GetStepDescription(i) ecalCharacterizer.AcquireStep(i) MsgBox "Acquire is complete" Next MsgBox "Now the user characterization will be saved to the ECal module and to PNA disk memory" ' Save the user characterization to the ECal module's memory. ' Note that this can take multiple minutes, depending on how ' many sweep points the channel has. ecalCharacterizer.SaveToECal ' Save the user characterization to PNA Disk Memory. Dim characterizationName characterizationName = "test" ecalCharacterizer.SaveToDiskMemory(characterizationName) MsgBox "User characterization is complete. Now we will calibrate using it. First we will use it from ECal module memory." Dim moduleMemCalKitName moduleMemCalKitName = GetCalKitName("User " & CStr(ecalCharacterizer.CharacterizationNumber)) DoTwoPortCal moduleMemCalKitName MsgBox "Now we will calibrate using the characterization from PNA Disk Memory." Dim pnaDiskMemCalKitName pnaDiskMemCalKitName = GetCalKitName(characterizationName) DoTwoPortCal pnaDiskMemCalKitName MsgBox "Example has completed"
Function GetCalKitName(characterizationName) Dim calKitName calKitName = ecalModelNum If Len(characterizationName) > 0 Then calKitName = calKitName & " " & characterizationName calKitName = calKitName & " ECal " & ecalSerialNum GetCalKitName = calKitName End Function
Sub DoTwoPortCal(calKitName) ' Initialize guided cal to be performed on Channel 1. Dim guidedCal Set guidedCal = calMgr.GuidedCalibration guidedCal.Initialize 1, True ' Specify the DUT connector for each PNA port to be calibrated (DUT connector = ECal characterization's connector) guidedCal.ConnectorType(1) = "APC 3.5 male" guidedCal.ConnectorType(2) = "APC 3.5 male" ' Specify the "cal kit" for each of those ports guidedCal.CalKitType(1) = calKitName guidedCal.CalKitType(2) = calKitName ' We know this example will result in a calibration sequence of a single "connection step" Dim numSteps numSteps = guidedCal.GenerateSteps ' Acquire the cal connection step guidedCal.AcquireStep 1 ' Conclude the cal and turn it on guidedCal.GenerateErrorTerms End Sub |