This example sets Phase Reference Cal properties, then performs a Phase Reference calibration.
It is NOT necessary to create an SMC measurement before performing a remote Phase Reference Cal. It is necessary when performed from the user interface.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as PMAR.vbs. Learn how to setup and run the macro.
PhaseReferenceCalibration Object
See other COM Example Programs
|
Example Program: performs a phase reference calibration between 1Ghz to 10Ghz on Ports 1, 2, and 4. Set app = CreateObject("agilentpna835x.application") app.preset app.activechannel.hold 1 Set PhaseReferenceCal = app.GetCalManager().PhaseReferenceCalibration ' always call reset at the beginning of your cal PhaseReferenceCal.Reset PhaseReferenceCal.StartFrequency = 1e9 PhaseReferenceCal.StopFrequency = 10e9 ' Read serial numbers of connected phase references ' Into variant array refs = PhaseReferenceCal.GetConnectedPhaseReferences 'Change the following to your own phase reference name PhaseReferenceCal.PhaseReference = "MYPILOT44" PhaseReferenceCal.SourceAttenuator = 10 PhaseReferenceCal.Calset = "Remote Phase Reference" PhaseReferenceCal.ConnectorType = "APC 3.5 female" PhaseReferenceCal.CalKitType = "85052D" ' Perform the calibration on Port 4 (Port 1 and Port 2 are always included) PhaseReferenceCal.IncludePort(4) = true ' Uncomment the following line to use an unknown mixer ' to extend the phase reference cal down to 10 Mhz ' If an unknown mixer is used, then the start frequency is always 10 Mhz ' PhaseReferenceCal.IncludeUnknownMixer = true Set guidedCal = PhaseReferenceCal.GuidedCalibration Steps = guidedCal.GenerateSteps for i = 1 to steps Msgbox guidedCal.GetStepDescription(i) guidedCal.AcquireStep i next msgbox guidedCal.GenerateErrorTerms msgbox "done" |
Last Modified:
|
24-Apr-2013 |
Updated for A.09.90 |
|
3-Apr-2012 |
MX New topic |