This VBScript example creates a Noise Figure Converter measurement for a converter with an Embedded LO.
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save it on the PNA hard drive as Noise.vbs. Learn how to setup and run the macro.
|
option explicit dim app dim chan dim host set app = CreateObject("Agilentpna835x.application") app.reset ' create NFX traces app.CreateCustomMeasurementEx 1, "Noise Figure Converters", "NF", 1 app.CreateCustomMeasurementEx 1, "Noise Figure Converters", "SC21", 1 'set channel and application objects set chan = app.ActiveChannel dim nfx set nfx = chan.CustomChannelConfiguration dim converter set converter = chan.GetConverter() dim calMgr set calMgr = app.GetCalManager dim nfxCal set nfxCal = CalMgr.CreateCustomCalEx(1) dim nfxCalExt set nfxCalExt = nfxCal.CustomCalConfiguration dim ELO set ELO = converter.ConverterEmbeddedLO ' Set embedded LO properties ELO.NormalizePoint = 101 ELO.TuningMode = 0 ' Broadband and precise ELO. TuningIFBW = 3.0e4 ELO.MaxPreciseTuningIterations = 5 ELO.PreciseTuningTolerance = 1 ELO.TuningSweepInterval = 1 ELO.IsOn = true 'The following single sweep performs the same 'function as "Find Now" on the ELO dialog chan.Single 1
|
Last Modified:
|
16-Aug-2012 |
Added Find now comment |
|
27-Oct-2009 |
MX New topic |