The following VB Script example exercises the COM commands used to setup Receiver Leveling.
RxLevelingConfiguration Object
See Other COM Example Programs
This VBScript (*.vbs) program can be run as a macro in the PNA. To do this, copy the following code into a text editor file such as Notepad and save on the PNA hard drive as RxLevel.vbs. Learn how to setup and run the macro.
|
' Demonstrate some COM commands for Receiver Leveling. Dim pna Set pna = CreateObject("AgilentPNA835x.Application") Dim chan Set chan = pna.ActiveChannel Dim RxLevel Set RxLevel = chan.GetRxLevelingConfiguration Dim srcPort srcPort = 1 pna.Preset RxLevel.ReferenceReceiver(srcPort) = "R1" RxLevel.Tolerance(srcPort)= 0.02 RxLevel.IterationNumber(srcPort)= 10 RxLevel.FastMode(srcPort)=True RxLevel.LevelingIFBW(srcPort)= 100 RxLevel.PowerOffset(srcPort)= 0 RxLevel.PowerMax(srcPort)= 20 RxLevel.PowerMin(srcPort)= -50 RxLevel.SafeMode(srcPort)= True RxLevel.State(srcPort)= True |
Last Modified:
|
1328-Jan-2011 |
MX New topic |