Write-only |
About Triggering |
Description |
Ends the current measurement sweep on the channel. |
VB Syntax |
chan.Abort [sync] |
Variable |
(Type) - Description |
|
chan |
(object) - A Channel object |
|
sync |
(boolean) - wait (or not) for the analyzer to stop before processing subsequent commands. Optional argument; if unspecified, value is set to False. Choose from: |
Return Type |
None |
Default |
None |
Examples |
chan.abort True |
C++ Syntax |
HRESULT Abort(VARIANT_BOOL bSynchronize); |
Interface |
IChannel |