Write-only
About ECAL Confidence Check

AcquireCalConfidenceCheckECAL Method - Superseded


Description

Note: This property is replaced by AcquireCalConfidenceCheckECALex Method

Transfers confidence data from the specified ECal module into the measurement's memory trace. The data is  transferred to the specified S-parameter on the same channel as this Calibrator object.

 The characterization within the ECal module that the confidence data will be read from is specified by the ECALCharacterization property on the ICalibrator2 interface.  The default value of the ECALCharacterization property is naECALFactoryCharacterization.

 VB Syntax

cal.AcquireCalConfidenceCheckECAL Sparam[,ecalModule]


Variable

(Type) - Description

cal

A Calibrator (object)

Sparam

(String) S-parameter to transfer confidence data to. This parameter must be present on the same channel as the calibrator object.

ecalModule

(enum NAECALModule) – Optional argument.  ECal module. Choose from:

0 - naECALModule_A (default, if unspecified)

1 - naECALModule_B

Return Type

None

Default

Not applicable


Examples

Cal.AcquireCalConfidenceCheckECAL "S11", naECALModule_A


C++ Syntax

HRESULT AcquireCalConfidenceCheckECAL( _bstr_t strParameter, enum NAECALModule ecalModule );

Interface

ICalibrator