Write-only |
About Source Power Cal |
Description |
This command replaces AcquirePowerReadings Method Initiates a source power cal acquisition. |
VB Syntax |
powerCalibrator.AcquirePowerReadingsEx calMethod, acqdevice [,sync] |
Variable |
(Type) - Description |
|
powerCalibrator |
(object) - A SourcePowerCalibrator object |
|
calMethod |
(enum NASourcePowerCalMethod) Selects the calibration method to be used for the source power cal acquisition. 0 – naPowerMeter Use power meter for all readings. 1 - naPowerMeterAndReceiver Power meter for the first iteration; then use the reference receiver for remaining readings if necessary. 2 - naReceiver Use PNA measurement receiver for all readings. |
|
acqdevice
|
(String) The specific acquisition device to be used. NOT case sensitive. Choose from: If calMethod = naPowerMeter or naPowerMeterAndReceiver, choose from:
If calMethod = naReceiver, choose from:
|
|
[sync]
|
(boolean) Optional argument. If not specified, value is set to False. Choose from: True (1) – The method does not return until this acquisition has completed (the program calling this method is halted while waiting for the method to return). False (0) – The method initiates an acquisition then returns immediately (while the acquisition still proceeds). The program calling this method can then perform other operations during the acquisition. |
Return Type |
None |
Default |
Not Applicable |
Examples |
powerCalibrator.AcquirePowerReadingsEx naPowerMeter, "asen", True powerCalibrator.AcquirePowerReadingsEx naReceiver, "b2" powerCalibrator.AcquirePowerReadingsEx naReceiver, "MyPMAR" |
C++ Syntax |
HRESULT AcquirePowerReadingsEx (tagNASourcePowerCalMethod enumCalMethod, BSTR bstrAcqDevice, VARIANT_BOOL bSync); |
Interface |
ISourcePowerCalibrator4 |
Last modified:
|
10-Feb-2011 |
Added PMAR |
|
9/12/06 |
MQ New command to accommodate receiver only SPC |