Write/Read
About Analyzer Events

AllowEventMessage Method


Description

Sets event filtering to monitor specific events.

 VB Syntax

app.AllowEventMessage event

Variable

(Type) - Description

app

An Application (object)

event

Event to monitor. Refer to list in Working with the Analyzer's Events

state

(boolean)
True
- monitor
False
- do not monitor

Return Type

Not Applicable

Default

Not Applicable

Examples

app.AllowEventMessage

C++ Syntax

HRESULT AllowEventMessage( tagNAEventID eventID, VARIANT_BOOL bAllow)

Interface

IApplication