Write-only
About Source Power Cal

ApplyPowerCorrectionValuesEx Method


Description

This command replaces ApplyPowerCorrectionValues Method.

Applies the array of power correction values to the channel memory and turns correction ON. Perform after completing a source power cal acquisition sweep.

This command does NOT save the correction values. To save correction values, save an instrument / calibration state (*.cst file) after performing a source power cal.

Optionally, as part of the source power calibration, perform calibration of the reference receiver used in the power calibration. Learn more.

 VB Syntax

powerCalibrator.ApplyPowerCorrectionValuesEX [rRec]

Variable

(Type) - Description

powerCalibrator

(object) - A SourcePowerCalibrator object

rRec

 (Enum as NASourcePowerApplyCorrectionOption) Optional argument. Choose from:

0 - naSourcePowerApplyCorrectionDefault  Do NOT perform and save a calibration of the reference receiver. (Default if not specified).

1 - naIncludeReferenceReceiverPowerCal  Perform and save a calibration of the reference receiver. The Cal Set, which includes only the reference receiver cal, is saved to the destination specified by RemoteCalStoragePreference.

Return Type

None

Default

Not Applicable

Examples

powerCalibrator.ApplyPowerCorrectionValuesEX

powerCalibrator.ApplyPowerCorrectionValuesEX (naIncludeReferenceReceiverPowerCal)

C++ Syntax

HRESULT ApplyPowerCorrectionValuesEx(enum NASourcePowerApplyCorrectionOption option);

Interface

ISourcePowerCalibrator5