Write-only | 
About Source Power Calibration | 
Description | 
 Copies and applies an existing Source Power Calibration to another channel.  | 
VB Syntax | 
 chan.ApplySourcePowerCalibrationTo (fromPortNum, targetChan, targetPortNum);  | 
Variable | 
(Type) - Description | 
| 
 chan  | 
 A Channel (object)  | 
| 
 fromPortNum  | 
 (Long) Port number of the existing source power correction.  | 
| 
 targetChan  | 
 (Long) Channel number to which the source power correction will be copied.  | 
| 
 targetPortNum  | 
 (Long) Port number to which the source power correction will be applied.  | 
Return Type | 
 Not Applicable  | 
Default | 
 Not Applicable  | 
Examples | 
 chan.ApplySourcePowerCalibrationTo 1,2,1  | 
C++ Syntax | 
 HRESULT ApplySourcePowerCalibrationTo (long fromPortNumber, long otherChannelNumber, long portNumber);  | 
Interface | 
 IChannel11  |