Write-only |
About Cal Plane Manager |
Description |
Characterizes a single fixture based on two existing calsets. To characterize two adapter/fixtures (on the input AND output of a fixture), perform this operation twice. |
VB Syntax |
calmgr.CharacterizeFixture (tier1Cset, tier2Cset, portNum, s2pFile, format, [dcPhase]) |
Variable |
(Type) - Description |
|
calMgr |
Cal Manager (Object) |
|
tier1Cset |
(String) Name of Tier-1 calset. The Tier-1 calset MUST be from a calibration that was performed at the input to the adapter/fixture. |
|
tier2Cset |
(String) Name of Tier-2 calset. The Tier-2 calset MUST be from a calibration that was performed at the DUT reference plane. |
|
portNum |
(Long Integer) Port number of the calsets to use when the specified calsets are used to calibrate more than one port. |
|
s2pFile |
(String) Path and filename to which the S2P file is to be saved. |
|
format |
(Enum as NAPairedDataFormat) Format in which the data is to be saved to the S2P file. Choose from: 0 - naLogMagPhase 1 - naLinMagPhase 2 - naRealImaginary |
|
[dcPhase] |
(Integer) Optional argument. The projected phase of S21 at DC where it crosses the X-axis. Learn more. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
CalManager.CharacterizeFixture ("Tier1", "Tier2", 1,"C:\Users\PNA-ADMIN\AppData\Local\Keysight\Network Analyzer\CPM\FixtureA.s2p",1,0) |
C++ Syntax |
HRESULT CharacterizeFixture(BSTR strCset1, BSTR strCset2, long pNum, BSTR fileName, tagNAPairedDataFormat format, Int dcPhase); |
Interface |
ICalManager10 |
Last Modified:
|
27-Jan-2014 |
MN New topic |