Write-only
About Cal Sets

CloseCalSet Method  Superseded


Description

This command is no longer necessary. The CalSet.get... and put... commands that required this command have been replaced,

Closes read/write access to the Cal Set.

See OpenCalSet for an explanation of gaining access to the Cal Set.

When you are finished reading and writing data from or to the Cal Set, close the Cal Set. Subsequent read/writes will require a new OpenCal Set call.

Reading and writing Cal Set data is performed with the PutStandard, GetStandard, PutErrorTerm, GetErrorTerm method calls. These methods are provided by the ICal Set and ICalData2 interfaces.

VB Syntax

CalSet.CloseCalSet

Variable

(Type) - Description

CalSet

(object) -  A Cal Set object

Return Type

Not Applicable

Default

Not Applicable

Examples

CSet.CloseCalSet

C++ Syntax

HRESULT CloseCalSet

Interface

ICalSet