Write-only
About Cal Sets

ComputeErrorTerms Method


Description

Computes error terms for the caltype specified by a preceding OpenCal Set call.

 The Cal Set must first be opened using OpenCalSet. If this call has not been made, the following error is issued:

E_NA_Cal Set_ACCESS_DENIED

The standards data required for the CalType must be available in the Cal Set or this error will be returned: E_NA_STANDARD_NOT_FOUND.

Note:  Error term computation requires data for the actual calibration kit standards from the current kit definition. ComputeErrorTerms assumes that the standards were acquired using only one standard per class.

VB Syntax

CalSet.ComputeErrorTerms

Variable

(Type) - Description

CalSet

(object) -  A Cal Set object

Return Type

Not Applicable

Default

Not Applicable

Examples

CalSet.ComputeErrorTerms

C++ Syntax

HRESULT ComputeErrorTerms( )

Interface

ICalSet