Read-only
About User Characterization

GetEcalUserCharacterizer Method


Description

This method returns a handle to an ECalUserCharacterizer object.

 VB Syntax

calMgr.GetEcalUserCharacterizer( )

Variable

(Type) - Description

calMgr

A CalManager Object (object)

Return Type

IEcalUserCharacterizer

Default

Not Applicable

Example

Dim mgr as ICalManager
Set mgr = app.GetCalManager
Dim ecalCharacterizer
Set ecalCharacterizer = mgr.GetECalUserCharacterizer()

C++ Syntax

HRESULT GetEcalUserCharacterizer( IECalUserCharacterizer **obj);

Interface

ICalManager6