Read-only
About VISAPassthrough

GetVISATimeout Method


Description

Returns the timeout value (in milliseconds) for pass-through commands for the specified VISA session.

VB Syntax

value = Vpassthru.GetVISATimeout (visaID)

Variable

(Type) - Description

value

(long) - Variable to store the returned value of the timeout.

Vpassthru

(object) -  A VISAPassthrough object

visaID

(long) - VISA session number (see Open method).

Return Type

Long

Default

Not Applicable

Examples

value=Vpassthru.GetVISATimeout(2)

C++ Syntax

HRESULT GetVISATimeout(long session_num)

Interface

IVISAPassthrough