Read-only |
About Cal Sets |
Description |
Returns a string identifying the Cal Set currently in use by the specified channel. This method identifies the Cal Set being used by returning its GUID. This method also identifies the "Error Term set" within the Cal Set. Error term sets are identified by integers, with set 0 belonging to the original (non-interpolated) terms. As stimulus values for a channel are changed causing interpolation to be required, a new Error Term set is constructed within the Cal Set to hold the interpolated Error Terms. The sets are sequentially numbered 1, 2, 3, and so forth. These Error Term sets are destroyed when they are no longer being used. If there is no Cal Set in use for the given channel, the <GUID> argument is set to the empty string. |
VB Syntax |
calMgr.GetCalSetUsageInfo chan, GUID, setNumber |
Variable |
(Type) - Description |
|
calMgr |
(object) - A CalManager object |
|
chan |
(long) - channel of the Cal Set being requested |
|
GUID |
(string) - variable to store the GUID of the Cal Set being requested. If there is no Cal Set in use for the given channel, the <GUID> argument is set to the empty string. |
|
setNumber |
(long) - variable to store the error term ID being requested. If the returned argument is greater than 0, the set is being interpolated. |
Return Type |
String, Long Integer |
Default |
Not Applicable |
Example |
calMgr.GetCalSetUsageInfo 1,GUID,EtermID |
C++ Syntax |
HRESULT GetCalSetUsageInfo (long lChannel, BSTR* CalSetGUID, long* etermSetID); |
Interface |
ICalManager |
Last Modified:
|
13-May-2011 |
Removed parens |