Read-only |
About Cal Sets |
Description |
Returns a string containing the GUID identifying this Cal Set. Each Cal Set is assigned a GUID (global unique ID). GUIDs are used to retrieve and select Cal Sets on the PNA. Learn more about reading and writing Cal Data using COM. |
VB Syntax |
value = CalSet.GetGuid |
Variable |
(Type) - Description |
|
value |
(string) - Variable to store the returned GUID |
|
CalSet |
(object) - A Cal Set object |
Return Type |
String |
Default |
Not Applicable |
Examples |
guid = CalSet.GetGuid 'Read |
C++ Syntax |
HRESULT GetGUID( BSTR* pGUIDString); |
Interface |
ICalSet |