Read-only |
Data Access Map |
Description |
Retrieves scalar data (ONE number per data point) from the specified location. Note: This method exists on a non-default interface. If you cannot access this method, use the Get Data Method on IMeasurement. |
VB Syntax |
measData.getScalar location, format, numPts, data |
Variable |
(Type) - Description |
|
measData |
An IArrayTransfer interface which supports the Measurement object |
|
location |
(enum NADataStore) - Where the data you want is residing. Choose from: 0 - naRawData 1 - naCorrectedData 2 - naMeasResult 3 - naRawMemory 4 - naMemoryResult 5 - naDivisor - When reading data from, or writing data to, the normalization divisor, you must first create a divisor trace using DataToDivisor Method. |
|
format |
(enum NADataFormat) - Format in which you would like the data. Choose from: 0 - naDataFormat_LinMag 1 - naDataFormat_LogMag 2 - naDataFormat_Phase 3 - naDataFormat_Polar 4 - naDataFormat_Smith 5 - naDataFormat_Delay 6 - naDataFormat_Real 7 - naDataFormat_Imaginary 8 - naDataFormat_SWR 9 - naDataFormat_PhaseUnwrapped 10 - naDataFormat_InverseSmith 11 - naDataFormat_Kelvin 12 - naDataFormat_Fahrenheit 13 - naDataFormat_Centigrade Note: Polar, Smith, and Inverse Smith are invalid formats for this command. See Get Complex Method. |
|
numPts |
(long integer) - Number of data points requested |
|
data |
(single) - Array to store the scalar data. |
Return Type |
Single |
Default |
Not Applicable |
Examples |
Dim dScalar() As Single |
C++ Syntax |
HRESULT getScalar(tagNADataStore DataStore, tagNADataFormat DataFormat, long* pNumValues, float* pVals) |
Interface |
IArrayTransfer |
Last Modified:
|
1-Oct-2007 |
Added temperature formats |