Write-only |
About Triggering |
Description |
Puts the channel in Hold - not sweeping. See chans.Hold to put ALL channels in hold. |
VB Syntax |
chan.Hold [sync] |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
[sync] |
The [sync] argument is ignored. Program control ALWAYS waits until the channel is in the Hold state. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
chan.Hold |
C++ Syntax |
HRESULT Hold |
Interface |
IChannel |
Last Modified:
|
20-Apr-2010 |
Updated sync |