Write-only |
About Triggering |
Description |
Sets the number of trigger signals the channel will receive. After the channel has received that number of trigger signals, the channel switches to Hold mode. |
VB Syntax |
chan.NumberOfGroups num, sync |
Variable |
(Type) - Description |
|
chan |
A Channel (object) |
|
num |
(long integer) Number of trigger signals the channel will receive. Choose any number between 1 and 2 million. |
|
sync |
(boolean) Variable set to either: True - subsequent commands are not processed until the groups are complete. Do not use with manual trigger. False - subsequent commands are processed immediately. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
chan.NumberOfGroups 5,False |
C++ Syntax |
HRESULT NumberOfGroups(long count, VARIANT_BOOL bWait) |
Interface |
IChannel |