Write-only |
Data Access Map |
Description |
Puts complex data into the specified location. This method forces the channel into Hold mode to prevent the input data from being overwritten. |
VB Syntax |
meas.putDataComplex location, data |
Variable |
(Type) - Description |
|
meas |
A measurement (object) |
|
location |
(enum NADataStore) Where the Data will be put. Choose from: 0 - naRawData 1 - naCorrectedData 2 - naMeasResult - Valid ONLY when the display format is either Polar or Smith Chart. 3 - naRawMemory - See note below. 4 - naMemoryResult 5 - naDivisor - When reading data from, or writing data to, the normalization divisor, you must first create a divisor trace using DataToDivisor Method.
Note: When putting data into 3 - naRawMemory: 1. Put the analyzer in hold mode 2. Call DataToMemory to initialize a memory buffer 3. Call putDataComplex(naRawMemory, data) This ensures that the memory buffer is appropriately initialized before receiving new data. |
|
data |
(variant) - A two-dimensional variant array. Note: All buffers except naMeasResult and naMemoryResult require Complex data |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
' Put 201 points worth of raw (complex) data into the measurement |
C++ Syntax |
HRESULT putDataComplex(tagNADataStore DataStore, VARIANT complexData) |
Interface |
IMeasurement |
Last Modified:
|
7-Aug-2012 |
Added naMeasResult note (DS) |