Write-only |
Data Access Map |
Description |
Puts formatted variant scalar data into the measurement result buffer. The data will be immediately processed and displayed. Subsequent changes to the measurement state will be reflected on the display. Always precede this command by setting the format on the measurement to be consistent with the format of the data being sent to the analyzer. In this way, the display annotation will be correct. Execution of this command does not change the display format. |
VB Syntax |
meas.putDataScalar format, data |
Variable |
(Type) - Description |
|
meas |
A measurement (object) |
|
format |
(enum NADataFormat) Format of the data. This value is presently ignored by the PNA. Data is always presented in the current format. Choose from: 0 - naDataFormat_LinMag 1 - naDataFormat_LogMag 2 - naDataFormat_Phase 3 - naDataFormat_Polar 4 - naDataFormat_Smith 5 - naDataFormat_Delay 6 - naDataFormat_Real 7 - naDataFormat_Imaginary 8 - naDataFormat_SWR 9 - naDataFormat_PhaseUnwrapped 10 - naDataFormat_InverseSmith 11 - naDataFormat_Kelvin 12 - naDataFormat_Fahrenheit 13 - naDataFormat_Centigrade Notes:
|
|
data |
(variant) - A 1-dimension array of single precision floating point numbers. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
' Put 201 points worth of scalar data into the measurement |
C++ Syntax |
HRESULT putDataScalar(tagNADataStore DataStore, VARIANT scalarArray) |
Interface |
IMeasurement |
Last Modified:
|
1-Oct-2007 |
Added temperature formats |