Write-only |
Data Access Map |
Description |
Puts Scalar data in the Measurement Result buffer. The putScalar array is not processed by the analyzer; it is just displayed. Any change to the measurement state (changing the format, for example) will cause the putScalar data to be overwritten with the data processed from the raw data buffer. |
VB Syntax |
measData.putScalar, format, numPts, data |
Variable |
(Type) - Description |
|
measData |
An IArrayTransfer interface which supports the Measurement object. |
|
format |
(enum NADataFormat) Format of the data. Choose from: 0 - naDataFormat_LinMag 1 - naDataFormat_LogMag 2 - naDataFormat_Phase 3 - naDataFormat_Polar 4 - naDataFormat_Smith 5 - naDataFormat_Delay 6 - naDataFormat_Real 7 - naDataFormat_Imaginary 8 - naDataFormat_SWR 9 - naDataFormat_PhaseUnwrapped 10 - naDataFormat_InverseSmith 11 - naDataFormat_Kelvin 12 - naDataFormat_Fahrenheit 13 - naDataFormat_Centigrade
Note: Smith, InverseSmith, and Polar formats are not allowed. |
|
numPts |
(integer) - Number of values. Usually the number of points in the trace (chan.NumberOfPoints). |
|
data |
(single) - A one-dimensional array of Scalar data matching the number of points in the current measurement. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
Dim measData As IArrayTransfer |
C++ Syntax |
HRESULT putScalar/(tagDataFormat eFormat, long lNumValues, float* pArrayOfScalar) |
Interface |
IArrayTransfer |
Last Modified:
|
1-Oct-2007 |
Added temperature formats |