Write-only |
About Macros |
Description |
Defines a Macro (shortcut) file in the analyzer. This command links a file name and path to the Macro file. The file must be put in the PNA at the location indicated by this command. |
VB Syntax |
app.PutShortcut index,title,path, arguments |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
index |
(long) - Number of the macro to be stored in the analyzer. Use a number between 1 and 25. If the index number already exists, the existing macro is replaced with the new macro. |
|
title |
(string) - The name to be assigned to the macro |
|
path |
(string) - Full path, file name, and extension of the existing macro "executable" file. |
|
arguments |
(string) - Arguments that may be required for the specified macro to run. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.PutShortcut 1,"Test","C:/Automation/MyTest.vbs","" |
C++ Syntax |
HRESULT PutShortcut(long Number, BSTR title, BSTR pathname,BSTR arguments) |
Interface |
IApplication |
Last Modified:
|
29-Apr-2013 |
Updated total to 25 |
|
25-Jun-2009 |
Added arguments |