Read-only
About VISAPassthrough

ReadString Method


Description

Returns data from the VISA pass-through device.

VB Syntax

value = Vpassthru.ReadString (visaID)

Variable

(Type) - Description

value

(string) - Variable to store the returned string data.

Vpassthru

(object) -  A VISAPassthrough object

visaID

(long) VISA session number (see Open method).

Return Type

String

Default

Not Applicable

Examples

value=Vpassthru.ReadString(1)

C++ Syntax

HRESULT ReadString(long session_num)

Interface

IVISAPassthrough