Write-only
About Modifying Cal Kits

Recall Kits Method


Description

Recalls the calibration kits definitions that were stored with the SaveKits command.

 VB Syntax

app.RecallKits

Variable

(Type) - Description

app

An Application (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

app.RecallKits

C++ Syntax

HRESULT RecallKits()

Interface

IApplication