Read-only |
|
Description |
E836x and PNA-L: Reads voltages on the DAC/Analog Output 1|2 of the Auxiliary IO connector. PNA-X: Reads voltage on the Power I/O connector AnalogOut1|2. |
VB Syntax |
volts = AuxIO.get_OutputVoltage (output) |
Variable |
(Type) - Description |
volts |
(double) - variable to store the return value |
AuxIO |
(object) - A Hardware Auxiliary Input / Output object |
output |
(variant) Number of the output DAC from which to read voltage. Choose from: 1 Output 1 (Aux I/O pin 3) and (Power I/O pin 3) 2 Output 2 (Aux I/O pin 2) and (Power I/O pin 4) |
Return Type |
Double |
Default |
Not Applicable |
Examples |
Dim aux as HWAuxIO Set aux = PNA.getAuxIO volts = aux.get_OutputVoltage(1) 'read voltage from Analog Out 1 (Aux I/O pin3) or (Power I/O pin 3) |
C++ Syntax |
HRESULT get_OutputVoltage( VARIANT Output, double* Voltage ); |
Interface |
IHWAuxIO |