Read-only |
|
Description |
Reads a 4-bit value from Port C of the Aux I/O connector (pins 22-25) and the Material Handler IO (pins 21-24 Anritsu) - (pins 22-25 Avantest). Note: These lines are connected to both the Handler IO and Aux IO in the PNA. |
VB Syntax |
value = AuxIO.get_PortCData |
Variable |
(Type) - Description |
|
value |
(variant) - Variable to store the returned data |
|
AuxIO |
(object) - A Hardware Auxiliary Input / Output object |
Return Type |
Integer |
Default |
None |
Examples |
value = auxIo.get_PortCData 'Reading a value of 15 when in Positive Logic indicates Port C lines C0, C1, C2, C3 are High. If in Negative Logic they are Low. |
C++ Syntax |
HRESULT get_PortCData( VARIANT* Data ); |
Interface |
IHWAuxIO |