| Description | This command sets the mode of the selected "Analog Out" line on the Power I/O connector. The modes give the user the option to have the requested voltage applied immediately or not until the sweep is done. To read the mode on each output use get_OutputVoltageMode Method. | 
| VB Syntax | auxIo.put_OutputVoltageMode (output, mode) | 
| Variable | (Type) - Description | 
| auxIo | (Object) An AuxIO object | 
| output | Analog Output to receive mode setting. Choose from 1 or 2 | 
| mode | (enum NAOutputVoltageMode ) naWaitEOS - While in this mode any voltage changes sent to the selected analog out will only get applied to the output between sweeps. naNoWait - While in this mode any voltage changes sent to the selected analog out will occur right away without waiting until the end of a sweep, the voltage gets applied immediately. | 
| Return Type | NAOutputVoltageMode | 
| Default | naWaitEOS | 
| Examples | auxIo.put_OutputVoltageMode 1, naWaitEOS 'Write | 
| C++ Syntax | HRESULT put_OutputVoltageMode(VARIANT Output, tagNAOutputVoltageMode dNewMode); | 
| Interface | IHWAuxIO |