Write-only |
|
Description |
Writes a 4-bit value to Port C on the Aux I/O connector (pins 22-25) and the Material Handler IO (pins 21-24 Anritsu) - (pins 22-25 Avantest). Note: These lines are connected to both the Handler IO and Aux IO in the PNA. Therefore, this command will affect both of these connectors in the same way. |
VB Syntax |
AuxIO.put_PortCData num |
Variable |
(Type) - Description |
|
AuxIO |
(object) - A Hardware Auxiliary Input / Output object |
|
num |
(variant) - 4 bit binary value. Choose from 0-15 |
Return Type |
None |
Default |
None |
Examples |
HWAuxIO.put_PortCData 15 'If Positive Logic, Port C lines C0, C1, C2, C3 go High. If Negative Logic, they go Low. |
C++ Syntax |
HRESULT put_PortCData( VARIANT Data ); |
Interface |
IHWAuxIO |