Provide commands for creating an equation.
Learn more about Equation Editor
Dim app As AgilentPNA835x.Application
Set app = CreateObject("AgilentPNA835x.Application", <analyzerName>)
Dim eq As Equation
Set eq = app.ActiveMeasurement.Equation
Methods |
Interface |
Description |
|---|---|---|
IMeasurementEquation2 |
Returns the functions in an imported (loaded) DLL. |
|
IMeasurementEquation2 |
Imports an Equation Editor DLL. |
|
IMeasurementEquation2 |
Returns whether a DLL has been imported into the PNA. |
|
IMeasurementEquation2 |
Removes an imported an Equation Editor DLL from the PNA. |
|
Properties |
Interface |
Description |
IMeasurementEquation |
Sets the Equation |
|
IMeasurementEquation |
Sets the Equation enabled state |
|
IMeasurementEquation |
Returns whether the equation is presently valid. |
Dim na Dim meas Set na = CreateObject("AgilentPNA835x.Application") Set meas = na.ActiveMeasurement 'Define the measurement meas.Equation.Text = "mysillyequ=sqrt(AR1_1)" 'Check to see if the equation is valid valid_e = meas.Equation.Valid MsgBox valid_e 'Turn on the Equation Editor meas.Equation.State = True |
Interface |
Introduced with PNA Rev: |
IMeasurementEquation |
6.03 |
IMeasurementEquation2 |
|
Last Modified:
1-Feb-2019 |
Changed IEquation to IMeasurementEquation |
4-Dec-2007 |
Added example |