Write / Read |
About Source Ports |
Description |
Sets and returns the ALC mode for the specified channel and port. Use GetSupportedALCModes to return a list of valid ALC modes for the PNA. |
VB Syntax |
chan.ALCLevelingMode (sourcePort) = value |
Variable |
(Type) - Description |
|
chan |
(object) - A Channel object |
|
sourcePort |
(long integer) - The source port for which to make this setting. If ports are remapped, specify the logical port number. Note: If the port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-x model, then you must use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port. |
|
value |
(enum as naALCLevelingMode) - Choose from:
|
Return Type |
Enum |
Default |
naALCInternal |
Examples |
chan.ALCLevelingMode(1) = 2 'Write |
C++ Syntax |
HRESULT get_ALCLevelingMode(long port, tagNAALCLevelingMode* pVal); HRESULT put_ALCLevelingMode(long port,tagNAALCLevelingMode newVal); |
Interface |
IChannel9 |