Write / Read | 
		About Display Colors | 
	
Description | 
		Set and return the labels and grid frame colors in the active window for the PNA display or hardcopy print. (Active labels, Grid frame)  | 
	
VB Syntax | 
		colors.ActiveLabels = value  | 
	
Variable | 
		(Type) - Description | 
	
colors  | 
		A ComColors (object)  | 
	
value  | 
		(Long Integer) - RGB color of the ActiveLabels pen. Convert the three RGB colors to an integer as follows: RGB = R+(G*2^8)+(B*2^16) To find the three RGB values from the Display Colors dialog, click Change Color, then Define Custom Color.  | 
	
Return Type | 
		Long  | 
	
Default | 
		Display = 175,175,175 Print = 0,0,0 (Black)  | 
	
Examples | 
		R = 10  | 
	
C++ Syntax | 
		HRESULT get_ActiveLabels(long* pVal); HRESULT put_ActiveLabels(long newVal);  | 
	
Interface | 
		IColors  |