Write/Read
About GCA Analysis

AnalysisCWFreq Property


Description

Set and return the CW frequency for a compression analysis trace.

 VB Syntax

gcaMeas.AnalysisCWFreq = value

Variable

(Type) - Description

gcaMeas

A GainCompressionMeas (object)

value

(Double)  CW frequency in Hz. Choose a frequency within the range of the gain compression channel.

Return Type

Double

Default

Not Applicable

Examples

gcaMeas.AnalysisCWFreq = 1e9 'Write

cwfreq = gca.AnalysisCWFreq 'Read

C++ Syntax

HRESULT get_AnalysisCWFreq(Double* value)

HRESULT put_AnalysisCWFreq(Double  value)

Interface

IGainCompressionMeas