Write/Read
About GCA Analysis

AnalysisXAxis Property


Description

Sets and returns the type of data to display on the x-axis of a compression analysis trace.

 VB Syntax

gcaMeas.AnalysisXAxis = value

Variable

(Type) - Description

gcaMeas

A GainCompressionMeas (object)

value

(Enum as NAGCAAnalysisXAxis)  Choose from:

naPsourceAsXAxis (0) - Power from the source.

naPinAsXAxis (1) - Input power to the DUT.

Return Type

Enum

Default

naPinAsXAxis (1)

Examples

gcaMeas.AnalysisXAxis = naPinAsXAxis 'Write

xAxis = gca.AnalysisXAxis 'Read

C++ Syntax

HRESULT get_AnalysisXAxis(tagNAGCAAnalysisXAxis* value)

HRESULT put_AnalysisXAxis(tagNAGCAAnalysisXAxis  value)

Interface

IGainCompressionMeas