Read-only

Application Property


Description

Returns the name of the Analyzer making measurements on the channel.

 VB Syntax

chan.Application

Variable

(Type) - Description

chan

A Channel (object)

Return Type

object

Default

None

Examples

rfna = chan.Application 'returns the Analyzer name

C++ Syntax

HRESULT get_Application(IApplication** Application)

Interface

IChannel