Write/Read
About Auto Port Extensions

AutoPortExtConfig Property


Description

Sets the frequency span that is used to calculate Automatic Port Extension. Learn more about calculating Automatic Port Extension.

 VB Syntax

fixture.AutoPortExtConfig  = value

Variable

(Type) - Description

fixture

A Fixturing (object)

value

(ENUM as NAAutoPortExtConfig)

0 naAPEC_CSPN  - Use current span.

1 naAPEC_AMKR  - Use active marker frequency.

2 naAPEC_USPN - Use custom user span. Use AutoPortExtSearchStart Property and AutoPortExtSearchStop Property to specify start and stop frequency.

Return Type

ENUM

Default

0 naAPEC_CSPN

Examples

fixture.AutoPortExtConfig = naAPEC_AMKR

value = fixture.AutoPortExtConfig 'Read

C++ Syntax

HRESULT get_AutoPortExtConfig(tagNAAutoPortExtConfig *pVal );

HRESULT put_AutoPortExtConfig(tagNAAutoPortExtConfig Val );

Interface

IFixturing2